Corporate NewsTransportation NewsIndustrial NewsAerospace & Defense NewsNewsletters

For more information, please contact:

Lori Appel
Manager, Marketing Communications

Kavlico
T 805-552-3406
F 805-523-7125
lappel@kavlico.com

Kavlico Publishes New Data Sheets for Aerospace Applications

May 22, 2008

MOORPARK, Calif. – Kavlico, a global business unit of Custom Sensors & Technologies (CST), has just release two new (2-sided, 8.5 x 11) data sheets that provide product information for the Aerospace & Defense markets.

The data sheets are:

  • GA Model – Landing Gear Control (LGC)
  • Pressure Sensors for Aerospace Applications &ndash including combined pressure & temperature
  • GA Model – Steering Handwheel

The brochures are available as a PDF on the Kavlico website at: http://www.kavlico.com/pages/library/product_literature.htm

The GA Model LGC data sheet includes a product a product photo and product description, a list of features and pertinent operating specifications. An electrical schematic is also provided.

The Pressure Sensor data sheet includes product photos, a brief description as well as an extensive list of features as well as a listing of typical applications. In addition, the data sheet has an extensive breakdown of operating specifications which includes such items as pressure range, proof pressure, burst pressure, output voltage, operating temperature, shock and vibration specs, housing material and electrical and pressure port interface options.

The GA Model Steering Handwheel data sheet includes product photos and product description,
a list of features and pertinent operating specifications. An electrical schematic is also provided.

All three sheets are available as downloadable PDFs on the Kavlico website in the Library at: http://www.kavlico.com/pages/library/product_literature.htm

Or, you can request a hard copy of the brochure via e-mail at: info@kavlico.com

About Kavlico

Kavlico is an operation of Custom Sensors & technologies (CST) and is a global business unit of Schneider Electric. Kavlico is a leading manufacturer of pressure, position (LVDT & RVDT), force, level, tilt, media quality, and other specialty sensors, and transducers for the transportation, industrial and aerospace & defense markets. www.kavlico.com

About Custom Sensors & Technologies

Headquartered in Moorpark, CA – Custom Sensors & Technologies (CST) is a global business unit of Schneider Electric and is comprised of industry-leading brands including Crouzet, Kavlico, Crydom, and former divisions of BEI Technologies – Newall and Systron Donner. CST provides sensors, controls, and actuation products for the Transportation, Industrial and Aerospace & Defense markets. www.cstsensors.com

Email Newsletter icon, E-mail Newsletter icon, Email List icon, E-mail List icon

Signup for our industry newsletter.

Constant Contact SafeSubscribe