Corporate NewsTransportation NewsIndustrial NewsAerospace & Defense NewsNewsletters

For more information, please contact:

Adrienne Warren
awarren@systron.com

Systron Donner Inertial Introduces New MEMS-Based Vertical Gyro (MMQ-VG) and Attitude, Heading, and Reference System (MMQ-AHRS)

June 20, 2008

Systron Donner Inertial Introduces New MEMS-Based Vertical Gyro (MMQ-VG) and Attitude, Heading, and Reference System (MMQ-AHRS)

Walnut Creek, CA – Systron Donner Inertial (SDI), a global business unit of Custom Sensors & Technologies (CST), is pleased to introduce their new MEMS-based Vertical Gyro (MMQ-VG) and Attitude, Heading, and Reference System (MMQ-AHRS).

These two new products MMQ-VG and MMQ-AHRS are fully functional Quartz MEMS sensor-based systems housed in a compact and light weight package. At the heart of each unit is SDI’s Six-Degree-of-Freedom MEMS Inertial Measurement Unit (IMU) which provides a highly accurate Roll, Pitch, and Heading (AHRS only) angle solution in varying dynamic conditions. Roll and Pitch are stabilized by the IMU accelerometers and heading is stabilized by an external three-axis magnetometer. The Vertical Gyro meets TSO-C4c Bank and Pitch angle requirements while the AHRS meets TSO-C4c as well as TSO-C6D Heading performance standards all the while providing the ultimate in MEMS rate sensor performance at 0.15 degrees/square root hour noise with stability under 10 degrees/hour.

The data output is user-configurable at various sample rates with extremely low output rate jitter. The easily understood data format contains six sensor outputs, the angle outputs, a Built-In-Test (BIT) word output, and a multi-parameter revolving word output providing system information including version string. The new SDI MMQ-VG and MMQ-AHRS combine outstanding performance and versatility within an extremely compact, low power consumption, and light-weight package.

About Systron Donner Inertial

Systron Donner Inertial (SDI) is an operation of Custom Sensors & Technologies (CST). SDI is a world leader in quartz MEMS inertial sensors and systems. SDI’s high performance products include rate sensors, multi-axis systems, IMUs and INS/GPS systems. www.systron.com

About Custom Sensors & Technologies

Headquartered in Moorpark, CA – Custom Sensors & Technologies (CST) is a global business unit of Schneider Electric and is comprised of industry-leading brands including Crouzet, Kavlico, Crydom, and former divisions of BEI Technologies – Newall and Systron Donner. CST provides sensors, controls, and actuation products for the Transportation, Industrial and Aerospace & Defense markets. www.cstsensors.com

Email Newsletter icon, E-mail Newsletter icon, Email List icon, E-mail List icon

Signup for our industry newsletter.

Constant Contact SafeSubscribe