For more information, please contact:
Lori Appel
Manager, Marketing Communications
Kavlico
T 805-552-3406
F 805-523-7125
lappel@kavlico.com
September 1, 2008
MOORPARK, Calif. – Kavlico, a global business unit of Custom Sensors & Technologies (CST) has released its new MAP sensor which utilizes a MEMS-based piezo-resistive (PRT) sense element. This new MAP sensor design is available in pressure ranges up to 3 Bar and has a light-weight plastic composite housing. Operating on 5 Vdc, the sensor provides a 0.5 to 4.5 Vdc analog output proportional to pressure standard with other custom outputs available.
Typically used in fuel injected engine management systems, MAP sensors provide instantaneous manifold pressure information to the engine’s electronic control unit (ECU). Air density is then calculated to determine the engine’s air mass flow rate which is then used to determine the optimum fuel flow to be delivered. By accurately metering the fuel flow, the vehicle runs more efficiently and economically, an imperative with today’s rising fuel cost.
Kavlico’s MAP sensors are high accuracy devices and have been fully temperature compensated across the entire operating range. Capable of withstanding high vibration environments, these sensors have excellent EMC performance. Small in size, the sensors can be specified with an integral temperature sensing option for increased functionality.
For high volume, OEM applications, Kavlico’s MAP sensors may be customized to suit each end-user’s application specific design criteria such as with a twist lock or fastener mount configuration.
Kavlico is an operation of Custom Sensors & technologies (CST) and is a global business unit of Schneider Electric. Kavlico is a leading manufacturer of pressure, position (LVDT & RVDT), force, level, tilt, media quality, and other specialty sensors, and transducers for the transportation, industrial and aerospace & defense markets. www.kavlico.com
Headquartered in Moorpark, CA – Custom Sensors & Technologies (CST) is a global business unit of Schneider Electric and is comprised of industry-leading brands including Crouzet, Kavlico, Crydom, and former divisions of BEI Technologies – Newall and Systron Donner. CST provides sensors, controls, and actuation products for the Transportation, Industrial and Aerospace & Defense markets. www.cstsensors.com