Corporate NewsTransportation NewsIndustrial NewsAerospace & Defense NewsNewsletters

For more information, please contact:

Gabriela Miranda

Crydom
T 619-210-1556
gabriela.miranda@crydom.com

Or visit our web site
www.crouzet.com

Crouzet Solid State Relay Operations Optimizes the Wiring Capabilities of the
GN Series SSRs

Crouzet GN series Solid State Relays now offer a clear plastic cover accepting larger size wire terminals while reducing the overall height of the relay

September 1, 2008

GN Series SSRs

Valence, France – Crouzet Solid State Relays, an operation of Custom Sensors & Technologies (CST), announces the improved GN series of solid state relays. Complying with the IEC IP20 touch safe regulation, the GN series now offer a clear plastic cover accepting larger size wire terminals suitable for up to #6 AWG wire and featuring an unrestricted view of wire installation. The overall height of the relay has also been reduced by 2 mm. Crouzet GN series solid state relays complying with the IEC IP00 regulation feature the same improvements as the IP20 versions, but without the clear IP20 protective cover.

The Crouzet GN series of relays have become a world wide benchmark for performance and reliability since their introduction 10 years ago. In response to customer requests to accept higher load current wire connections, Crouzet has improved the termination of the GN series while retaining all of their present features and benefits. Specifications, Part Numbers, Safety Agency Approvals, RoHS compliance and CE certifications of the improved offer remain identical to the previous offer. In addition, several new features are now available including an improved base plate for better thermal conductivity, easier removal of the IP20 cover with a standard #1 flat blade screw driver and a clear plastic cover for ease of wiring.

Requests for information or questions regarding the new GN series SSR offer should be sent directly to Crydom&rsqup;s customer service team or your preferred authorized Crouzet distributor.

About Crouzet

Crouzet, headquartered in France, has about 1800 employees with a presence in more than 40 countries. Now known as a specialist brand, Crouzet is focused on added value and customization for integrators and equipment manufacturers and serves markets such as medical, elevators and lifts, food processing, lighting, water treatment, entertainment, plastic injection/extrusion and office equipment. Crouzet brand SSRs are manufactured by Crydom Inc., a subsidiary company of Custom Sensors and Technologies.
www.crouzet.com
www.crouzet-usa.com

About Crydom

Crydom is an operation of Custom Sensors & Technologies (CST). Crydom is the global leader in solid state relay technology. Crydom manufactures and sells two of the most preferred brands of solid state relays around the world, Crydom and Crouzet. Thousands of catalog off-the-shelf items are available, as well as custom-designed solid state relays and related products. Crydom continues to satisfy the most demanding customers’ environmental and performance requirements creating product solutions to suit their specific application. www.crydom.com

About Custom Sensors & Technologies

Headquartered in Moorpark, Calif., Custom Sensors & Technologies (CST) is a business unit of Schneider Electric. CST was formed from the combination of Kavlico, Crouzet, Crydom and former divisions of BEI Technologies. CST provides sensors, controls and actuation products to the industrial, transportation, and military and aerospace markets. www.cstsensors.com

Email Newsletter icon, E-mail Newsletter icon, Email List icon, E-mail List icon

Signup for our industry newsletter.

Constant Contact SafeSubscribe