Corporate NewsTransportation NewsIndustrial NewsAerospace & Defense NewsNewsletters

For more information, please contact:

Lori Appel
Manager, Marketing Communications

Kavlico
T 805-552-3406
F 805-523-7125
lappel@kavlico.com

Kavlico Offers a Broad Selection of Pressure Sensors for HVAC & Refrigeration Applications

September 2, 2008

Broad Selection of Pressure Sensors for HVAC & Refrigeration Applications

MOORPARK, Calif. – Kavlico, a global business unit of Custom Sensors & Technologies (CST), has a full line of pressure sensors that address the needs of the HVAC/R industry. Manufactured for high volume, OEM applications, Kavlico pressure sensors provide accurate and repeatable pressure measurements for such applications as:

HVAC – variable air volume (VAV) systems, static duct pressure, filter pressure monitoring, combustion air flow, modulated furnace controls, and gaseous leak detection
Refrigeration – chillers, supermarket refrigeration, refrigerant suction & discharge monitoring, and hydronic systems and steam recovery

Low range differential pressures are available from 0-1 to 0-10“ H20 while gage and absolute versions are available in pressure ranges up to 6,000 psi. The sensors require a supply voltage of 5 Vdc and provide a 0.5 to 4.5 Vdc linear amplified output proportional to pressure for gage and absolute versions while the low range differential pressure sensors provide a 0.25 to 4.0 Vdc output.

Other significant features include EMI, RFI, and reverse polarity protection, excellent long-term stability, and low hysteresis. The sensors are available in a wide range of housing materials including stainless steel, brass, and plastic composite dependent upon product model number. A host of electrical and process connections, including a Schrader deflator are available to meet customer design specifications. All sensors are fully temperature compensated. Kavlico’s HVAC/R sensors are RoHS compliant and carry the CE mark.

These HVAC/R pressure sensors utilize a ceramic capacitive, capacitive MEMS or oil-filled piezoresistive (PRT) sense element. Private label sensors for high volume applications are also available.

About Kavlico

Kavlico is an operation of Custom Sensors & technologies (CST) and is a global business unit of Schneider Electric. Kavlico is a leading manufacturer of pressure, position (LVDT & RVDT), force, level, tilt, media quality, and other specialty sensors, and transducers for the transportation, industrial and aerospace & defense markets. www.kavlico.com

About Custom Sensors & Technologies

Headquartered in Moorpark, CA – Custom Sensors & Technologies (CST) is a global business unit of Schneider Electric and is comprised of industry-leading brands including Crouzet, Kavlico, Crydom, and former divisions of BEI Technologies – Newall and Systron Donner. CST provides sensors, controls, and actuation products for the Transportation, Industrial and Aerospace & Defense markets. www.cstsensors.com

Email Newsletter icon, E-mail Newsletter icon, Email List icon, E-mail List icon

Signup for our industry newsletter.

Constant Contact SafeSubscribe