For more information, please contact:
Lori Appel
Manager, Marketing Communications
Kavlico
T 805-552-3406
F 805-523-7125
lappel@kavlico.com
September 15, 2008
MOORPARK, Calif. – Kavlico, a global business unit of Custom Sensors & Technologies (CST), has just released an 8 page, 4-color capability brochure highlighting their OEM and catalog sensor product families for the industrial market sector.
Within the brochure is useful information detailing applications, custom design solutions, available sensing technologies, manufacturing and quality information. The brochure also has a sensor selection guide directing the reader based upon their application and measurement requirement to a range of applicable products via model number.
The main advantage of the new brochure is a handy 4-panel product reference matrix which can be wall-mounted for easy reference. The matrix depicts the model numbers with a product description and color photo across the top, while product specifications are delineated below in a grid format making it ideal for specification lookup. Specifications such as; pressure range, supply voltage, output, sensing technology, media compatibility, total error band, housing material, pressure and electrical connections are provided within the matrix.
The brochure is available as a PDF on the Kavlico website at: http://www.kavlico.com/pages/library/product_literature.htm
Or, you can request a hard copy of the brochure via e-mail at: sales@kavlico.com
Kavlico is an operation of Custom Sensors & technologies (CST) and is a global business unit of Schneider Electric. Kavlico is a leading manufacturer of pressure, position (LVDT & RVDT), force, level, tilt, media quality, and other specialty sensors, and transducers for the transportation, industrial and aerospace & defense markets. www.kavlico.com
Headquartered in Moorpark, CA – Custom Sensors & Technologies (CST) is a global business unit of Schneider Electric and is comprised of industry-leading brands including Crouzet, Kavlico, Crydom, and former divisions of BEI Technologies – Newall and Systron Donner. CST provides sensors, controls, and actuation products for the Transportation, Industrial and Aerospace & Defense markets.
www.cstsensors.com