For more information, please contact:
Lori Appel
Manager, Marketing Communications
Kavlico
T 805-552-3406
F 805-523-7125
lappel@kavlico.com
September 23, 2008
MOORPARK, Calif. – Kavlico, a global business unit of Custom Sensors & Technologies (CST), was deemed a certified supplier by Meggitt Aircraft Breaking Systems (MABS®) as a result of Kavlico’s excellent quality system. The quality award was presented in August for Kavlico’s Pedal Position Transducers. These non-contacting, all-stainless steel constructed, single-channel LVDT’s have a sleeve-over-sleeve design for telescopic movement.
These robustly designed, highly accurate sensors are packaged into Meggitt’s Flight Deck Brake Control Assemblies which are then installed on regional jets such as the CASA 295 and the Saab 2000 as well as business jets such as the Dassault Falcon 7X & Gulfstream G200 and G300/400, and the Hawker 4000.
MABS is one of the leading aircraft braking system suppliers, with facilities on both sides of the Atlantic, and in Asia. MABS provides aircraft braking equipment for commercial transport, business aviation and military aircraft.
Kavlico is an operation of Custom Sensors & technologies (CST) and is a global business unit of Schneider Electric. Kavlico is a leading manufacturer of pressure, position (LVDT & RVDT), force, level, tilt, media quality, and other specialty sensors, and transducers for the transportation, industrial and aerospace & defense markets. www.kavlico.com
Headquartered in Moorpark, CA – Custom Sensors & Technologies (CST) is a global business unit of Schneider Electric and is comprised of industry-leading brands including Crouzet, Kavlico, Crydom, and former divisions of BEI Technologies – Newall and Systron Donner. CST provides sensors, controls, and actuation products for the Transportation, Industrial and Aerospace & Defense markets. www.cstsensors.com