Corporate NewsTransportation NewsIndustrial NewsAerospace & Defense NewsNewsletters

For more information, please contact:

Keith Ayers

BEI Kimco Magnetics
T 760-597-6313
keith.ayers@beikimco.com

BEI Kimco Magnetics’ New Voice Coil Actuator Offers Improved Consistency And Precision In Valve Control And Beam Steering Applications

October 2, 2008

BEI Kimco Magnetics High Precision Integrated Motor Encoder Assembly for Extremely Fine Positioning

Vista, CA – BEI Kimco Magnetics, a company of Custom Sensors & Technologies (CST), has introduced a new compact sized, high force, cylindrical Voice Coil Actuator in response to market demand for improved consistency and precision in valve control and beam steering applications. Typical uses include analytical/test and measurement equipment for the pharmaceutical, R&D, laboratories, and medical industries.

Designed with high force sensitivity in a lightweight housing, the new actuator provides extremely fast control of valve opening and closing, thereby increasing throughput for OEMs looking to improve production and reduce product time to market. Used in conjunction with a high performance motion controller or other device, the actuator is capable of providing precise positioning, velocity, and acceleration in applications where exacting precision is critical.

The new actuator is available in small sizes from 1-inch OD to 1-1/2-inch OD for installation into products with tight space constraints. Features include stroke lengths ranging from 0 to 1.27 mm, force versus position curve characteristic, continuous force of 1 to 5 N, cog and hysteresis-free operation, and tight tolerances. The unit can be ordered in a variety of materials, allowing the OEM to select an actuator that is compatible with the type of sample being tested at the final point of use.

“Chemical compatibility is an important aspect for many of these types of applications,” explains Miguel Hermosillo, Application Sales Engineer for BEI Kimco. “To address this, BEI Kimco provides a variety of material choices for the customer to select from, thereby ensuring compatibility between the chemical being tested and the actuator itself.”

In addition to material choices, several other product configurations are available. Customers can select the lead, stroke length, voltage, shaft, and linear or rotary design that meets their specific application requirement. “This versatility allows us to meet the variety of anticipated customer requirements for unique uses,” adds Hermosillo.

The new actuator is competitively priced from $45.00 in production quantities with lead times of stock to eight weeks. For further information contact BEI Kimco Magnetics, 2470 Coral Street, Bldg. D, Vista, CA 92081-8430, USA, Tel: (760) 597-7042; Toll-free: (800) 572-7560; Fax: (760) 597-6320; sales@beikimco.com

About BEI Kimco Magnetics

BEI Kimco Magnetics is an operation of Custom Sensors & Technologies (CST). BEI Kimco Magnetics was founded in 1974 and specializes in rotary and linear motion control products. The company’s precision control products include high-speed performance Brushless DC motors, Cylindrical and Flat Voice Coil Actuators, and Linear Motors. These products are used across a wide range of applications including medical and scientific, factory and office automation, optics, semiconductor/electronics, military, aviation, space systems, and security. Kimco merges leading-edge capabilities and cost-effective manufacturing know-how with highly customized applications expertise.www.beikimco.com

About Custom Sensors & Technologies

Headquartered in Moorpark, CA – Custom Sensors & Technologies (CST) is a global business unit of Schneider Electric and is comprised of industry-leading brands including Crouzet, Kavlico, Crydom, and former divisions of BEI Technologies – Newall and Systron Donner. CST provides sensors, controls, and actuation products for the Transportation, Industrial and Aerospace & Defense markets. www.cstsensors.com

Email Newsletter icon, E-mail Newsletter icon, Email List icon, E-mail List icon

Signup for our industry newsletter.

Constant Contact SafeSubscribe