Corporate NewsTransportation NewsIndustrial NewsAerospace & Defense NewsNewsletters

For more information, please contact:

Sebastien Nobiron

Newall
T +44 (0) 116 264 2730
sebastien.nobiron@newall.co.uk

Newall Introduces New Generation of DRO Encoder

October 6, 2008

New Generation of DRO Encoder

Columbus, Ohio – Newall, a global business unit of Custom Sensors & Technologies (CST), has just introduced a new second generation linear encoder; the Spherosyn 2G. Designed for the conventional machine tool market, the Spherosyn 2G is quicker to install, requires no maintenance and comes with a five year warranty on the encoder and a lifetime warranty on the scales.

Newall’s linear encoder and scales technology is unique and provides consistent accuracy even under the harshest working environments. The new Spherosyn 2G encoder has completely new electronics and offers a significantly reduced total cost of ownership compared to its predecessor. The new internals enable more accurate alignment, which makes installation easier and 30–50% quicker than traditional technologies such as glass and magnetic tape.

With all the electronics encased in a new tough metal reader head, the Spherosyn 2G encoder and stainless steel scales require no maintenance whatsoever. The bushing technology and no mechanical wear characteristics mean it is extremely durable and reliable, giving minimal machine downtime.

Unlike glass scales which require regular cleaning and are susceptible to scratches or breaks, Newall’s robust stainless steel scales do not suffer from contamination problems and therefore don’t have to been cleaned or replaced. This alone can save thousands of pounds a year in machine shop overheads.

This latest addition to the Newall range is the only encoder on the market to offer a five year warranty and Newall’s scales now carry a lifetime guarantee such is the company’s confidence in the reliability of their product.

The Spherosyn 2G has the same foot print as the older Spherosyn and the same signal. This makes the 2G compatible with the many thousands of the older Spherosyn encoders in the field and any of the Newall DRO displays.

Managing director, Sebastien Nobiron, comments, “We are very proud of this new generation linear encoder which is made here in our UK facility. The advances our engineers have achieved with the Spherosyn 2G have provided customers with a more cost effective, higher performance, reliable and aesthetically designed product. The new curved body is not only stronger and more robust, but it’s also more effective with long scale support kits.”

“Another great benefit for the customer is the complete lack of need for maintenance and this is further enhanced by our new five year warranty on the encoder and lifetime warranty on scales,” continues Nobiron.

“Our delivery levels are excellent too. We provide 48 hour delivery on any length of scale, which is significantly better than other manufacturers whose delivery times can stretch up to 6 weeks for certain lengths. And, of course, we offer excellent technical support throughout the UK,” he concludes.

About Newall

Newall Measurement Systems, Ltd. was founded in 1968 in Peterborough, United Kingdom. Since that time Newall has dedicated itself to providing the machine tool and other machinery and production industries with leading edge technologies that increase productivity and machine tool efficiency. Over the years, Newall has grown to be a well-respected leader in digital readout systems and linear encoder technology. Over 85% of Newall’s products are exported, with distribution and service outlets in over 63 countries. www.newall.com.

About Custom Sensors & Technologies

Headquartered in Moorpark, CA – Custom Sensors & Technologies (CST) is a global business unit of Schneider Electric and is comprised of industry-leading brands including Crouzet, Kavlico, Crydom, and former divisions of BEI Technologies – Newall and Systron Donner. CST provides sensors, controls, and actuation products for the Transportation, Industrial and Aerospace & Defense markets. www.cstsensors.com

Email Newsletter icon, E-mail Newsletter icon, Email List icon, E-mail List icon

Signup for our industry newsletter.

Constant Contact SafeSubscribe