For more information, please contact:
Lori Appel
Manager, Marketing Communications
Kavlico
T 805-552-3406
F 805-523-7125
lappel@kavlico.com
October 7, 2008
MOORPARK, Calif. – Kavlico, a global business unit of Custom Sensors & Technologies (CST), has developed two new, high accuracy, low-pressure sensors for pressure measurement applications in next generation modulated furnaces. The model P992 is ideally suited to measure airflow, while the P356 measures propane or natural gas flow.
The rapid escalation of energy costs over the past several years has “fueled” a new urgency to improve the efficiency of residential and commercial heating systems. Kavlico’s high precision pressure sensors provide furnace controls suppliers with a device that assists with combustion optimization parameters making the furnace efficiency jump from 65% to 95%.
The sensors are fully temperature compensated and can be adapted to meet application-specific OEM requirements.
Kavlico is an operation of Custom Sensors & technologies (CST) and is a global business unit of Schneider Electric. Kavlico is a leading manufacturer of pressure, position (LVDT & RVDT), force, level, tilt, media quality, and other specialty sensors, and transducers for the transportation, industrial and aerospace & defense markets. www.kavlico.com
Headquartered in Moorpark, CA – Custom Sensors & Technologies (CST) is a global business unit of Schneider Electric and is comprised of industry-leading brands including Crouzet, Kavlico, Crydom, and former divisions of BEI Technologies – Newall and Systron Donner. CST provides sensors, controls, and actuation products for the Transportation, Industrial and Aerospace & Defense markets. www.cstsensors.com