For more information, please contact:
Lori Appel
Manager, Marketing Communications
Kavlico
T 805-552-3406
F 805-523-7125
lappel@kavlico.com
November 12, 2008

MOORPARK, Calif. – Kavlico, a global business unit of Custom Sensors & Technologies (CST), has recently introduced the P6060 high accuracy pressure sensors that are suitable for air pressure measurements in:
These rugged, lightweight (1.3 grams Max.) devices have a piezo-reseitive (PRT) sense element in a low-profile surface mount package. Small in size, the sensors measure 21.29 x 16.71 mm.
Using a 5 volt input, the sensors provide a 0.5 to 4.5 Vdc linear analog amplified output proportional to pressure. The user has the option to specify a digital output that conforms to SPI protocol.
Internal temperature compensation using a state-of-the-art ASIC insures an accurate ±1% of span total error band (TEB) over 0 to +60°C. Available pressure ranges include 13" H20 and 0–1 through 0–75 PSIA, PSIG, and PSID.
The easy-to-use P6060 sensors are EMI/RFI and ESD protected, experience no mounting position effects and provide a fast response. The sensors can be configured with custom pressure ranges and port connections dependent upon the end-users application-specific requirements.
For applications that do not require a ±1% accuracy, the P6050 pressure sensors is available with a ±2% TEB specification over temperature. As an additional benefit, the sensors are RoHS compliant.
Kavlico is an operation of Custom Sensors & technologies (CST). Kavlico is a leading manufacturer of pressure, position (LVDT & RVDT), force, level, tilt, media quality, and other specialty sensors, and transducers for the transportation, industrial and aerospace & defense markets. www.kavlico.com
Headquartered in Moorpark, CA, Custom Sensors & Technologies (CST) unit is comprised of the industry-leading brands of Crouzet, Kavlico, Crydom, as well as the former divisions of BEI Technologies, including Newall and Systron Donner. CST provides sensors, controls, and actuation products for the transportation, industrial and aerospace & defense markets. www.cstsensors.com