For more information, please contact:
Lori Appel
Manager, Marketing Communications
Kavlico
T 805-552-3406
F 805-523-7125
lappel@kavlico.com
November 20, 2008

MOORPARK, Calif. – Kavlico, a global business unit of Custom Sensors & Technologies (CST), has just published three Data Sheets for their recently released industrial pressure sensor products; the P500, the P250/P251, and the P250R/P251R.
Each Data Sheet Includes:
The Data Sheets are available as downloadable PDF files on the Kavlico website in the Resource Center.
The P500 High Performance OEM Pressure Sensors
The P250/P251 Sealed Industrial Pressure Sensors
The P250R/P25R Sealed Industrial Pressure Sensors with Internal Regulator
Kavlico industrial pressure sensors are available in off-the-shelf options as well as custom designed for high volume OEM’s application-specific requirements. For more information about Kavlico pressure sensor solutions for the transportation, industrial, and aerospace & defense markets, visit the Kavlico website.
Kavlico is an operation of Custom Sensors & technologies (CST). Kavlico is a leading manufacturer of pressure, position (LVDT & RVDT), force, level, tilt, media quality, and other specialty sensors, and transducers for the transportation, industrial and aerospace & defense markets. www.kavlico.com
Headquartered in Moorpark, CA, Custom Sensors & Technologies (CST) unit is comprised of the industry-leading brands of Crouzet, Kavlico, Crydom, as well as the former divisions of BEI Technologies, including Newall and Systron Donner. CST provides sensors, controls, and actuation products for the transportation, industrial and aerospace & defense markets. www.cstsensors.com