For more information, please contact:
Lori Appel
Manager, Marketing Communications
Kavlico
T 805-552-3406
F 805-523-7125
lappel@kavlico.com
November 21, 2008
MOORPARK, Calif. – Kavlico, a global business unit of Custom Sensors & Technologies (CST), published “10 reasons to use a… Pressure Sensor Checklist” in the November issue of Design World Magazine. Co-authored by two of Kavlico’s finest; Steve Smith, Director of Transportation Sales, Western Region & Asia and Gary Casey, Director of Product Development, Transportation, the article is a “How to Guide” for selecting pressure sensors that meet the end-users application.
The checklist highlights ten significant factors one should review prior to deciding upon the type of pressure sensor to design into the end-use application. The Pressure Sensor “pre-flight” Checklist should include:
It is vital to make sure that each of the above parameters is understood and specified correctly to ensure that the sensor selected and ultimately purchased and installed is the right sensor for the application. For those who are looking for some useful guidelines to assist with selecting pressure sensors, check out the Pressure Sensor Checklist.
Kavlico is an operation of Custom Sensors & technologies (CST). Kavlico is a leading manufacturer of pressure, position (LVDT & RVDT), force, level, tilt, media quality, and other specialty sensors, and transducers for the transportation, industrial and aerospace & defense markets. www.kavlico.com
Headquartered in Moorpark, CA, Custom Sensors & Technologies (CST) unit is comprised of the industry-leading brands of Crouzet, Kavlico, Crydom, as well as the former divisions of BEI Technologies, including Newall and Systron Donner. CST provides sensors, controls, and actuation products for the transportation, industrial and aerospace & defense markets. www.cstsensors.com