Corporate NewsTransportation NewsIndustrial NewsAerospace & Defense NewsNewsletters

For more information, please contact:

Lori Appel
Manager, Marketing Communications

Kavlico
T 805-552-3406
F 805-523-7125
lappel@kavlico.com

Kavlico Has a Full Line of Sensors for Refrigeration Pressure Applications

December 8, 2008

Refrigeration Pressure Sensors

MOORPARK, Calif. – Kavlico, a global business unit of Custom Sensors & Technologies (CST), has a full line of pressure sensors specifically designed to address the needs of the refrigeration market. Name the application, and Kavlico can deliver the right pressure sensor to fit the broad spectrum of volume vs. cost target requirements. Whether the application calls for measuring chiller pressure, supermarket refrigeration, refrigerant suction and discharge, or hydronic system pressure and steam recovery, Kavlico sensors have been designed to perform.

Popular Kavlico sensor models for refrigeration applications include:

  • P158 Refrigeration Pressure Sensor
  • P528 High Volume Refrigeration Pressure Sensor
  • P4000 Sealed High Pressure Sensor
  • PT250/PT251 Sealed Industrial Pressure Transmitter
  • P250/P251 Sealed Industrial Pressure Sensor
  • P250R/P251R Sealed Industrial Pressure Sensors with Internal Regulator

The high accuracy (±2% Total Error Band over -15 to +85°C) refrigeration sensors feature either a rugged brass or stainless steel housing and can be specified with a wide variety of electrical and pressure port connection to fit each unique application.

The sensors have high overpressure capability, and can operate in high shock, vibration and humidity environments. EMI/RFI protected, the sensors also feature over-voltage, reverse polarity, and short circuit protection. Temperature compensated over a wide operating range, the sensors have a ten million cycle life expectancy. Output options include linear amplified 0.5 to 4.5 Vdc, 0 – 5 and 0 – 10 Vdc regulated, or a current output of 4 – 20mA.

About Kavlico

Kavlico is an operation of Custom Sensors & technologies (CST). Kavlico is a leading manufacturer of pressure, position (LVDT & RVDT), force, level, tilt, media quality, and other specialty sensors, and transducers for the transportation, industrial and aerospace & defense markets. www.kavlico.com

About Custom Sensors & Technologies

Headquartered in Moorpark, CA, Custom Sensors & Technologies (CST) unit is comprised of the industry-leading brands of Crouzet, Kavlico, Crydom, as well as the former divisions of BEI Technologies, including Newall and Systron Donner. CST provides sensors, controls, and actuation products for the transportation, industrial and aerospace & defense markets. www.cstsensors.com

Email Newsletter icon, E-mail Newsletter icon, Email List icon, E-mail List icon

Signup for our industry newsletter.

Constant Contact SafeSubscribe