For more information, please contact:
Lori Appel
Manager, Marketing Communications
Kavlico
T 805-552-3406
F 805-523-7125
lappel@kavlico.com
February 2, 2009

MOORPARK, Calif. – Kavlico, a global business unit of Custom Sensors & Technologies (CST) has designed the P356 low pressure gage/differential pressure sensor for applications requiring long-term stability and an operational life in excess of ten years.
Typical applications include:
Available in pressure ranges of 0–0.5, 0–1, ±1, 0–3, and 0–5 PSI, the P356 provides a linear amplified voltage output proportional to pressure of 0.5 through 4.5 Vdc from a 5 Vdc regulated power supply. Featuring a brass housing and excellent EMI protection, this device has a response time of <10m sec and an operating temperature range of -20° to +125°C. Built-in reverse polarity and over-voltage protection allow for ease of installation while excellent hysteresis, repeatability, and linearity provide accurate measurement.
The P356 is packaged for high volume applications requiring a rugged, compact design while offering flexible configuration options for application-specific requirements. Key to the sensor’s high performance and low cost is Kavlico’s ceramic, variable capacitive sensing element and integral ASIC with hybrid circuit for reliable signal conditioning.
Kavlico is an operation of Custom Sensors & technologies (CST). Kavlico is a leading manufacturer of pressure, position (LVDT & RVDT), force, level, tilt, media quality, and other specialty sensors, and transducers for the transportation, industrial and aerospace & defense markets. www.kavlico.com
Headquartered in Moorpark, CA, Custom Sensors & Technologies (CST) unit is comprised of the industry-leading brands of Crouzet, Kavlico, Crydom, as well as the former divisions of BEI Technologies, including Newall and Systron Donner. CST provides sensors, controls, and actuation products for the transportation, industrial and aerospace & defense markets. www.cstsensors.com