Corporate NewsTransportation NewsIndustrial NewsAerospace & Defense NewsNewsletters

For more information, please contact:

Lori Appel
Manager, Marketing Communications

Kavlico
T 805-552-3406
F 805-523-7125
lappel@kavlico.com

Kavlico General Purpose Pressure Sensor Utilizes a Mixed-Signal CMOS ASIC

February 9, 2009

Kavlico General Purpose Pressure Sensor

MOORPARK, Calif. – Kavlico, a global business unit of Custom Sensors & Technologies (CST) has developed the P255 general purpose pressure sensor with advanced electronics for enhanced performance. The mixed-signal CMOS ASIC provides for improved EMI/RFI and accuracy specifications. Specifically designed for pressure measurements of 0–15 to 0–1000 PSIA/PSIG, the P255 is a robust device utilizing a ceramic diaphragm that can withstand exposure to a wide array of liquid and gaseous process media.

Excited by 5 Vdc, the P255 provides a linear amplified output of 0.5 to 4.5 Vdc that is proportional to pressure. The sensor has low power consumption, superior long-term stability, and excellent repeatability and hysteresis. Other significant features include over-voltage, reverse polarity, and short circuit protection.

The P255 has a 316 stainless steel housing and has an operating temperature range of -40° to +125°C. Due to the sensors high shock and vibration tolerance, it is well suited for applications such as:

  • Hydraulic systems
  • Refrigeration and HVAC systems
  • Gas tank pressure monitoring
  • Level measurements
  • Coolant pressures
  • Agricultural chemical equipment
  • Marine systems
  • Aggressive fluid measurements

The P255 is RoHS compliant and can be ordered in off-the-shelf designs or adapted to fit unique OEM application-specific requirements. A wide variety of electrical connector and pressure connection ports may be chosen to fit measurement criteria.

About Kavlico

Kavlico is an operation of Custom Sensors & technologies (CST). Kavlico is a leading manufacturer of pressure, position (LVDT & RVDT), force, level, tilt, media quality, and other specialty sensors, and transducers for the transportation, industrial and aerospace & defense markets. www.kavlico.com

About Custom Sensors & Technologies

Headquartered in Moorpark, CA, Custom Sensors & Technologies (CST) unit is comprised of the industry-leading brands of Crouzet, Kavlico, Crydom, as well as the former divisions of BEI Technologies, including Newall and Systron Donner. CST provides sensors, controls, and actuation products for the transportation, industrial and aerospace & defense markets. www.cstsensors.com

Email Newsletter icon, E-mail Newsletter icon, Email List icon, E-mail List icon

Signup for our industry newsletter.

Constant Contact SafeSubscribe