For more information, please contact:
Adrienne Warren
awarren@systron.com
February 9, 2009
Walnut Creek, CA – Systron Donner Inertial (SDI), a company of Custom Sensors & Technologies (CST) has developed a low cost gyro; the LCG50, which incorporates a MEMS (Micro Electro Mechanical System) single axis angular rate sensor on a small PC board. The LCG50 Gyro is ideally suited for embedded applications where mounting versatility is required such as in guidance and control systems, robotics, flight testing, short term navigation, and vehicle instrumentation.
The high reliability LCG50 is a complete unit requiring only a DC voltage input to measure angular rate while providing an analog voltage output along with a wide bandwidth. The economical, environmentally robust sensor exhibits performance characteristics that match more expensive instrument grade rate sensors.
Additional features include a wide operating temperature range of -40 to +85°C, low power consumption, a fast start-up time of <2 sec typical, integral temperature sensor output, and a compact design with a weight of <0.4 oz. or 12 grams.
Standard Part Numbers & Ranges include:
Contact Systron Donner Inertial (SDI) for availability at: sales@systron.com
Systron Donner Inertial (SDI) is an operation of Custom Sensors & Technologies (CST). SDI is a world leader in quartz MEMS inertial sensors and systems. SDI’s high performance products include rate sensors, multi-axis systems, IMUs and INS/GPS systems. www.systron.com.
Headquartered in Moorpark, CA – Custom Sensors & Technologies (CST) is a global business unit of Schneider Electric and is comprised of industry-leading brands including Crouzet, Kavlico, Crydom, and former divisions of BEI Technologies – Newall and Systron Donner. CST provides sensors, controls, and actuation products for the Transportation, Industrial and Aerospace & Defense markets. www.cstsensors.com