For more information, please contact:
Lori Appel
Manager, Marketing Communications
Kavlico
T 805-552-3406
F 805-523-7125
lappel@kavlico.com
February 23, 2009

MOORPARK, Calif. – Kavlico, a global business unit of Custom Sensors & Technologies (CST) has designed a robust pressure sensor; the model P265, which utilizes a ceramic capacitive sense element that can withstand exposure to a wide array of compatible liquid and gaseous media. Housed in a 316 stainless steel package, the sensor is excited by 5Vdc and provides a linear amplified output of 0.5 to 4.5 Vdc that is proportional to pressure.
Specifically designed for pressure measurements of 0–15 through 0–1,000 PSIA/PSIG, the P265 has low power consumption, superior long-term stability, and excellent repeatability and hysteresis. Other significant features include over-voltage, reverse polarity, and short circuit protection. The P265 has an operating temperature range of -40° to +125°C.
The excellent shock and vibration tolerance of the P265 makes it an ideal fit for applications such as:
The P265 pressure sensor is available in many standard off-the-shelf configurations or it can be adapted to fit unique OEM application specific requirements. A wide selection of pressure ports and electrical connectors may be chosen to fit the measurement criteria.
Kavlico is an operation of Custom Sensors & technologies (CST). Kavlico is a leading manufacturer of pressure, position (LVDT & RVDT), force, level, tilt, media quality, and other specialty sensors, and transducers for the transportation, industrial and aerospace & defense markets. www.kavlico.com
Headquartered in Moorpark, CA, Custom Sensors & Technologies (CST) unit is comprised of the industry-leading brands of Crouzet, Kavlico, Crydom, as well as the former divisions of BEI Technologies, including Newall and Systron Donner. CST provides sensors, controls, and actuation products for the transportation, industrial and aerospace & defense markets. www.cstsensors.com