March 2, 2009
Columbus, Ohio – Newall’s cost effective B60 Milling Machine Digital Readout Package offers unprecedented value for turret and knee mills. The Digital Readout (DRO) is housed in a rugged die cast chassis and is available in two or three axis. A keypad ensures long life and the crisp and clear LEDs make it easy to read even at long distances and wide viewing angles.
The B60 incorporates Newall’s Spherosyn and Microsyn encoders that are recognized throughout the world for their quality, accuracy, and reliability. The package is covered by Newall’s unmatched 5-year warranty and 3-year no-fault warranty that covers accidental damage and mis-use. Measuring 9.5 x 5.5 x 2.2" (240 x 140 x 80mm), the B60 weighs 6.3 lbs. or 2.9 kg.
In addition to the B60, Newall also offers the M20 Milling Package, another cost-effective milling machine solution.
Newall Measurement Systems, Ltd. was founded in 1968 in Peterborough, United Kingdom. Since that time Newall has dedicated itself to providing the machine tool and other machinery and production industries with leading edge technologies that increase productivity and machine tool efficiency. Over the years, Newall has grown to be a well-respected leader in digital readout systems and linear encoder technology. Over 85% of Newall’s products are exported, with distribution and service outlets in over 63 countries. www.newall.com.
Headquartered in Moorpark, CA, Custom Sensors & Technologies (CST) unit is comprised of the industry-leading brands of Crouzet, Kavlico, Crydom, as well as the former divisions of BEI Technologies, including Newall and Systron Donner. CST provides sensors, controls, and actuation products for the transportation, industrial and aerospace & defense markets. www.cstsensors.com