Corporate NewsTransportation NewsIndustrial NewsAerospace & Defense NewsNewsletters

For more information, please contact:

Gabriela Miranda

Crydom
T 619-210-1556
gabriela.miranda@crydom.com

Crydom Announces The Addition Of 4 New High Power DC Output SSRs

New D1D and D2D series solid state relays add to Crydom’s already extensive offer for high-current DC applications such as heater, lighting and motor control

March 16, 2009

New D1D and D2D series solid state relays

San Diego, CA – Crydom’s D1D and D2D series of FET output DC Solid State Relays formerly rated up to 40 amps at 100 VDC and 12 amps at 200 VDC, now includes new models rated at 60, 80 and 100 amps at 100 VDC, as well as 40 amps at 200 VDC. The new models which are offered in the industry standard “hockey puck” SSR package, adds to Crydom’s present offer which includes the D06 rated to 100 amps at 60 VDC, D2D & D4D series rated to 12 amps and D5D models rated to 10 amps at 200, 400 and 500 VDC respectively.

The new D1D relays feature a low on-state resistance FET output capable of carrying 60, 80 or 100 amps when the SSR is mounted on an appropriately rated heat sink. Likewise, the new D2D40 features a similar FET design rated to 40 amps with appropriate heat sink. Control for these Crydom DC output SSRs is by a transformer isolated 3 to 32 VDC logic compatible input providing 2500 VAC input to output isolation. The outputs are diode protected and specified to operate up to 1 kHz.

About Crydom

Crydom is an operation of Custom Sensors & Technologies (CST). Crydom is the global leader in solid state relay technology. Crydom manufactures and sells two of the most preferred brands of solid state relays around the world, Crydom and Crouzet. Thousands of catalog off-the-shelf items are available, as well as custom-designed solid state relays and related products. Crydom continues to satisfy the most demanding customers’ environmental and performance requirements creating product solutions to suit their specific application. www.crydom.com

About Custom Sensors & Technologies

Moorpark, CA – Custom Sensors & Technologies (CST) is a global business unit of Schneider Electric and is comprised of industry-leading brands including Crouzet, Kavlico, Crydom, and former divisions of BEI Technologies – Newall and Systron Donner. CST provides sensors, controls, and actuation products for the Transportation, Industrial and Aerospace & Defense markets. www.cstsensors.com

Email Newsletter icon, E-mail Newsletter icon, Email List icon, E-mail List icon

Signup for our industry newsletter.

Constant Contact SafeSubscribe