For more information, please contact:
Lori Appel
Manager, Marketing Communications
Kavlico
T 805-552-3406
F 805-523-7125
lappel@kavlico.com
April 1, 2009

MOORPARK, Calif. – Kavlico, a global business unit of Custom Sensors & Technologies (CST) has a suite of sensors that have been designed to perform in a wide variety of hydraulic applications. Capable of operating for millions of pressure cycles, these low power consumption pressure sensors provide an accurate, reliable, and stable signal over many years of operation in the harshest environments. The high overpressure capability of our sensors for fluid power applications are designed to withstand the pressure fluctuations associated with these applications.
These rugged devices have stainless steel housings and can be configured with a broad selection of process and electrical connectors to fit the specification criteria for each application. Operating on 5 Vdc, the sensors provide a 0.5 to 4.5 linear amplified output proportional to pressure. Pressure ranges are available up to 6,000 PSI.
Kavlico is an operation of Custom Sensors & technologies (CST). Kavlico is a leading manufacturer of pressure, position (LVDT & RVDT), force, level, tilt, media quality, and other specialty sensors, and transducers for the transportation, industrial and aerospace & defense markets. www.kavlico.com
Headquartered in Moorpark, CA, Custom Sensors & Technologies (CST) unit is comprised of the industry-leading brands of Crouzet, Kavlico, Crydom, as well as the former divisions of BEI Technologies, including Newall and Systron Donner. CST provides sensors, controls, and actuation products for the transportation, industrial and aerospace & defense markets. www.cstsensors.com