Corporate NewsTransportation NewsIndustrial NewsAerospace & Defense NewsNewsletters

For more information, please contact:

Michelle Todd

BEI Industrial Encorders
T 800-350-2727
michelle.todd@cst.schneider-electric.com

Absolute Encoders Go Wireless with SwiftComm™

April 24, 2009

Absolute Encoders Go Wireless

GOLETA, Calif. – BEI Industrial Encoders introduces the SwiftComm Wireless Interface for SSI absolute encoders. No need to incur the expense and maintenance of long cable runs – go wireless! Using SSI communications protocol at the transmitter and receiver end, users can connect the wireless receiver directly into the SSI port in the controller, just like a conventional wired system. The interface works with any SSI position device; single or multi-turn encoders, linear scales, magnetostrictive devices or any other SSI sensor.

A robust and secure wireless interface, SwiftComm has the built-in reliability needed for real-time industrial control. Able to interface with any SSI absolute or incremental sensor, SwiftComm allows critical position and speed feedback data to be seamlessly sent to control systems without expensive cabling. The SwiftComm system includes the transmitter-receiver pair, which communicates using a point-to-point frequency-hopping 2.4 GHz RF protocol. SwiftComm is ideal for a wide variety of industrial applications where cable runs are expensive to install and maintain.

For more information, visit www.beiied.com/wireless.

About BEI Industrial Encoders

BEI Industrial Encoders (IED) is a company of Custom Sensors & Technologies (CST). IED manufactures optical encoders and associated electronics for the industrial market. IED is the market-leading brand of encoders in North America. http://www.beiied.com

About Custom Sensors & Technologies

Headquartered in Moorpark, CA – Custom Sensors & Technologies (CST) is comprised of industry-leading brands including Crouzet, Kavlico, Crydom, and former divisions of BEI Technologies – Newall and Systron Donner. CST provides sensors, controls, and actuation products for the Transportation, Industrial and Aerospace & Defense markets.http://www.cstsensors.com

Email Newsletter icon, E-mail Newsletter icon, Email List icon, E-mail List icon

Signup for our industry newsletter.

Constant Contact SafeSubscribe