Corporate NewsTransportation NewsIndustrial NewsAerospace & Defense NewsNewsletters

For more information, please contact:

Lori Appel
Manager, Marketing Communications

Custom Sensors & Technologies (CST)
T 805-552-3406
F 805-523-7125
lori.appel@cstsensors.com

CST Brands to Promote Sensors & Controls at 2009 Paris Air Show

May 1, 2009

MOORPARK, Calif. – Custom Sensors & Technologies (CST), and three of its industry-leading brands for aerospace & defense products will be exhibiting at the 2009 Paris Air Show in Le Bourget from June 15th through June 21st. The show will be celebrating 100 years and CST’s will be located in Hall 4, Stand 4-F102. The booth will feature a cockpit mock-up with instrument panel and both Crouzet and CST pilot input devices will be installed.

CST’s featured brands will be:

Crouzet – will be promoting their line of aerospace products including electrical protection devices (traditional circuit breakers, arc and ground fault circuit breakers, and solid state circuit breakers), Detection devices (proximity switches and sensors), as well as their cockpit devices (wheels and grips).

Kavlico – will feature the pressure sensors that measure pressures up to 30,000 PSI (2,100 Bar). Their highly reliable and accurate sensors are rugged by design and have been built for hostile environment, flight critical applications. The pressure sensors are available in both amplified and non-amplified versions, in wet or dry configurations, and are available in absolute or differential pressure ranges. In addition to their line of pressure sensors, Kavlico will have on display their position sensors (LVDT & RVDT), force sensors and their complete line of cockpit/pilot control devices.

Systron Donner Inertial (SDI) – will be featuring their inertial sensing products. On display will be three of their single axis rate gyros (QRS116, SDG500 and SDG1000). In addition, their SDI500 tactical grade performance IMU will be spotlighted. While at the show, visitors will learn about performance features of each product as well as typical applications.

According to Brad Smith, CST’s Vice President of Aerospace & Defense products, “The Paris Air Show provides CST with a platform to present new products and applications not only to potential new customers’, but to our existing customer base as well. The event represents the best the industry has to offer and it is truly an opportunity everyone in the aerospace industry should experience.”

About Crouzet

Crouzet, headquartered in France, has about 1800 employees with a presence in more than 40 countries. Now known as a specialist brand, Crouzet is focused on added value and customization for integrators and equipment manufacturers and serves markets such as medical, elevators and lifts, food processing, lighting, water treatment, entertainment, plastic injection/extrusion and office equipment. Crouzet brand SSRs are manufactured by Crydom Inc., a subsidiary company of Custom Sensors & Technologies. www.crouzet.com

About Kavlico

Kavlico is an operation of Custom Sensors & technologies (CST). Kavlico is a leading manufacturer of pressure, position (LVDT & RVDT), force, level, tilt, media quality, and other specialty sensors, and transducers for the transportation, industrial and aerospace & defense markets. www.kavlico.com

About Systron Donner Inertial

Systron Donner Inertial (SDI) is an operation of Custom Sensors & Technologies (CST). SDI is a world leader in quartz MEMS inertial sensors and systems. SDI’s high performance products include rate sensors, multi-axis systems, IMUs and INS/GPS systems. www.systron.com

About Custom Sensors & Technologies

Headquartered in Moorpark, CA, Custom Sensors & Technologies (CST) unit is comprised of the industry-leading brands of Crouzet, Kavlico, Crydom, as well as the former divisions of BEI Technologies, including Newall and Systron Donner. CST provides sensors, controls, and actuation products for the Transportation, Industrial and Aerospace & Defense markets. www.cstsensors.com

Email Newsletter icon, E-mail Newsletter icon, Email List icon, E-mail List icon

Signup for our industry newsletter.

Constant Contact SafeSubscribe