Corporate NewsTransportation NewsIndustrial NewsAerospace & Defense NewsNewsletters

For more information, please contact:

Keith Ayers

T 714-998-9255
Keith.ayers@beikimco.com

BEI Kimco Magnetics Provides Cog-Free Linear Voice Coil Servo Actuators

May 12, 2009

Cog-Free Linear Voice Coil Servo Actuators

Vista, CA – BEI Kimco Magnetics model LA15-16-020A is a two-wire non-commutated direct drive linear voice coil servo actuator motor featuring cog-free, hysteresis free motion with high acceleration capability. This 1.5-in diameter x 1.56-in. long device has a 0.4-in. stroke. It is rated at 2.6-lb. force continuous and 7.6-lb. force for 10 seconds. LA15-16-020A is a cost-effective, superior performance alternative to rotary-to-linear conversion servo drives.

The LA15-16-020A model is a 0.25-in. stroke linear voice coil actuator rated at 5.5-lb. force, continuous and 20.0-lb. force for 10 seconds. This two wire non-commutated actuator measuring 1.5-in. diameter x 1.56-in. long is hysteresis free, cog-free and has a simple linear control characteristic. It is a cost-effective high performance direct drive servo mechanism that exceeds the capabilities of rotary-to-linear conversion devices.

For further information, contact BEI Kimco Magnetics, 2470 Coral Street, Bldg. D, Vista, CA 92081-8430, USA, Tel: (760) 597-7042; Toll-free: (800) 572-7560; Fax: (760) 597-6320; Email: sales@beikimco.com.

About BEI Kimco Magnetics

BEI Kimco Magnetics is an operation of Custom Sensors & Technologies (CST). BEI Kimco Magnetics was founded in 1974 and specializes in rotary and linear motion control products. The company’s precision control products include high-speed performance Brushless DC motors, Cylindrical and Flat Voice Coil Actuators, and Linear Motors. These products are used across a wide range of applications including medical and scientific, factory and office automation, optics, semiconductor/electronics, military, aviation, space systems, and security. BEI Kimco merges leading-edge capabilities and cost-effective manufacturing know-how with highly customized applications expertise. www.beikimco.com

About Custom Sensors & Technologies

Headquartered in Moorpark, CA – Custom Sensors & Technologies (CST) is comprised of industry-leading brands including Crouzet, Kavlico, Crydom, and former divisions of BEI Technologies – Newall and Systron Donner. CST provides sensors, controls, and actuation products for the Transportation, Industrial and Aerospace & Defense markets. www.cstsensors.com

Email Newsletter icon, E-mail Newsletter icon, Email List icon, E-mail List icon

Signup for our industry newsletter.

Constant Contact SafeSubscribe