May 12, 2009
Vista, CA – BEI Kimco Magnetics the typical “inside-out” brushless DC (BLDC) motor provides greater output power, higher operating speeds and cleaner, quieter operation than its brush-type counterparts. BLDC motors are ideal for sterile environments—since there are no brushes, no particulate is discharged.
Because of their inherent reliability and long-term service life, BLDC brushless motors can significantly contribute to lower overall cost of operation and maintenance.
BEI Kimco Magnetics offers a comprehensive line of fractional horsepower brushless DC motors that are currently manufactured in sizes from 1.1" to 9.0" diameter capable of operating at speeds in excess of 60 KRPM.
Call us at 1-800-572-7560 to inquire about larger sizes and speeds.
BEI Kimco Standard Catalog Motor Products
For further information, contact BEI Kimco Magnetics, 2470 Coral Street, Bldg. D, Vista, CA 92081-8430, USA, Tel: (760) 597-7042; Toll-free: (800) 572-7560; Fax: (760) 597-6320; Email: sales@beikimco.com.
BEI Kimco Magnetics is an operation of Custom Sensors & Technologies (CST). BEI Kimco Magnetics was founded in 1974 and specializes in rotary and linear motion control products. The company’s precision control products include high-speed performance Brushless DC motors, Cylindrical and Flat Voice Coil Actuators, and Linear Motors. These products are used across a wide range of applications including medical and scientific, factory and office automation, optics, semiconductor/electronics, military, aviation, space systems, and security. BEI Kimco merges leading-edge capabilities and cost-effective manufacturing know-how with highly customized applications expertise. www.beikimco.com
Headquartered in Moorpark, CA – Custom Sensors & Technologies (CST) is comprised of industry-leading brands including Crouzet, Kavlico, Crydom, and former divisions of BEI Technologies – Newall and Systron Donner. CST provides sensors, controls, and actuation products for the Transportation, Industrial and Aerospace & Defense markets. www.cstsensors.com