For more information, please contact:
Michelle Todd
BEI Industrial Encorders
T 800-350-2727
michelle.todd@beisensors.com
June 1, 2009
GOLETA, Calif. – BEI Industrial Encoders’ new linear cable transducer provides digital position and speed feedback information in a rugged, easy-to-install package. Model LT25 cable transducer utilizes a flexible measuring cable mounted to an internal spring-loaded spool and a quadrature encoder output to precisely measure linear motion applications. The sturdy cable is made of nylon coated stainless steel for ultimate strength and has a measurement range up to 125 inches.
Easy to install, simply connect the LT25 cable to your moving equipment and secure the base to a fixed object. Hard to reach areas or worries about shaft misalignment are now not a problem. The LT25 cable transducer allows for easy reorientation of the mounting bracket or encoder connector position, giving users added adaptability to their installation. With an IP66 rating, the LT25 is a perfect solution for a variety of industrial measurement challenges including wet, dirty, or outdoor environments or applications where your measuring range travels over a harsh environment.
For more information, visit www.beiied.com/cable-transducer.
BEI Industrial Encoders (IED) is a company of Custom Sensors & Technologies (CST). IED manufactures optical encoders and associated electronics for the industrial market. IED is the market-leading brand of encoders in North America. http://www.beiied.com
Headquartered in Moorpark, CA – Custom Sensors & Technologies (CST) is comprised of industry-leading brands including Crouzet, Kavlico, Crydom, and former divisions of BEI Technologies – Newall and Systron Donner. CST provides sensors, controls, and actuation products for the Transportation, Industrial and Aerospace & Defense markets.http://www.cstsensors.com