Corporate NewsTransportation NewsIndustrial NewsAerospace & Defense NewsNewsletters

For more information, please contact:

Lori Appel
Manager, Marketing Communications

Kavlico
T 805-552-3406
F 805-523-7125
lappel@kavlico.com

Kavlico’s P528 OEM Pressure Sensor Incorporates an Integral Schrader Deflator Process Fitting for Refrigeration Applications

June 2, 2009

P528 OEM Pressure Sensor

MOORPARK, Calif. – Kavlico, a global business unit of Custom Sensors & Technologies (CST) has recently added the P528 OEM Refrigeration Pressure Sensor with a 1/4 SAE Female Flare, Schrader Deflator with 7/16-20 UNF internal threads to their P528 family of sensors. This sensor which incorporates Kavlico’s 4th generation ceramic capacitive sensing technology has been specifically engineered for high volume OEM refrigeration applications.

Packaged in a brass or stainless steel housing, the sensor can endure the high vibration, broad temperature ranges, and high humidity conditions found in refrigeration systems while withstanding high over-pressures and pressure pulsations without damage or degradation. Pressure ranges available are from 0 – 100 through 0 – 1,000 PSI absolute and sealed gage.

Typical refrigeration applications include:

  • High and Low Side Pressure Measurements in Refrigeration Systems
  • Product Refrigeration
  • Transport Refrigeration
  • Refrigerant Recovery
  • Environmental Test Equipment

The P528 is offered with seal materials that are compatible with many of the latest refrigerants such as R134a, R22, R123, R12, R410A as well as a host of the proprietary blends and associated lubricants.

The compact and lightweight sensor (<1.75" long and 50 grams max.) features an external hex for quick and easy installation. It operates on 5 Vdc and provides a linear amplified analog output of 0.5 to 4.5 Vdc proportional to pressure. The low power consumption device has superior long-term stability and is temperature compensated over the entire operating range. The operating temperature range is -30 to +135°C. The sensor is RoHS compliant and carries CE Mark certification.

About Kavlico

Kavlico is an operation of Custom Sensors & Technologies (CST). Kavlico is a leading manufacturer of pressure, position (LVDT & RVDT), force, level, tilt, media quality, and other specialty sensors, and transducers for the transportation, industrial and aerospace & defense markets. www.kavlico.com

About Custom Sensors & Technologies

Headquartered in Moorpark, CA, Custom Sensors & Technologies (CST) unit is comprised of the industry-leading brands of Crouzet, Kavlico, Crydom, as well as the former divisions of BEI Technologies, including Newall and Systron Donner. CST provides sensors, controls, and actuation products for the transportation, industrial and aerospace & defense markets. www.cstsensors.com

Email Newsletter icon, E-mail Newsletter icon, Email List icon, E-mail List icon

Signup for our industry newsletter.

Constant Contact SafeSubscribe