For more information, please contact:
Lori Appel
Manager, Marketing Communications
Kavlico
T 805-552-3406
F 805-523-7125
lappel@kavlico.com
June 22, 2009

MOORPARK, Calif. – Kavlico, a global business unit of Custom Sensors & Technologies (CST) is pleased to announce the availability of their 4th generation ceramic capacitive pressure sensor, the model P500 which is packaged with Kavlico’s state-of-the-art ASIC. Rugged and highly reliable, this multi-purpose sensor is ideal for measuring a broad range of process media including hydrocarbon based fluids, air, and water.
Typical industrial pressure sensor applications include:
Typical transportation applications include:
The extremely compact sensor (less than 50 grams in weight and <1.6" in length) can be packaged in brass, stainless steel or carbon plated steel dependent upon pressure range and measurement requirement. Standard pressure ranges are available from 0 – 15 through 0 – 750 PSI and 0–1 through 0–40 Bar, absolute or sealed gage.
Other significant features include outstanding shock and vibration performance, low power consumption, high over pressure protection, excellent EMI/RFI, and ESD protection, and a temperature compensated linear amplified output of 0.5 to 4.5 Vdc. Operating temperature is -40 to +125°C when using a fluorsilicone o-ring.
Standard packaging includes a built-in Metri-Pack 150 Series electrical connector although other options may be specified while the process connection may be specified with a variety of popular thread options. The Model P500 is RoHS compliant and carries CE Mark certification and is IP65 rated.
Kavlico is an operation of Custom Sensors & Technologies (CST). Kavlico is a leading manufacturer of pressure, position (LVDT & RVDT), force, level, tilt, media quality, and other specialty sensors, and transducers for the transportation, industrial and aerospace & defense markets. www.kavlico.com
Headquartered in Moorpark, CA, Custom Sensors & Technologies (CST) unit is comprised of the industry-leading brands of Crouzet, Kavlico, Crydom, as well as the former divisions of BEI Technologies, including Newall and Systron Donner. CST provides sensors, controls, and actuation products for the transportation, industrial and aerospace & defense markets. www.cstsensors.com