Corporate NewsTransportation NewsIndustrial NewsAerospace & Defense NewsNewsletters

For more information, please contact:

Laetitia Martin-Berne

Crouzet
T +33 (0)4 75 44 87 27
F +33 (0)4 75 44 86 40
laetitia.martin-berne@crouzet.com

Crouzet’s Programmable MTP05 Connects Directly to the Millenium 3

August 25, 2009

Programmable MTP05

Valence, France – Crouzet, a global business unit of Custom Sensors & Technologies (CST), is pleased to announce the availability of its latest programmable touch panel, which connects directly to the Millenium 3 via the programming port.

Measuring only 3.5", this ultra compact panel offers unparalleled display performance, with excellent visibility even when using small characters, high contrast, and superior brightness thanks to the high intensity LEDs.

Offering 2 MB memory capacity (for creating up to 180 screens), the MTP05 is easy to program and use, with the intuitive symbol library greatly simplifying the whole screen creation process.

Directly compatible with the Millenium 3 SLin/SLout blocks, this complete one-screen solution can control the Millenium 3 and vice versa.

The MTP05 Millenium 3 Touch Panel archives data on an SD card to save valuable time. And by locating numerous Millenium 3 display function blocks remotely in the MTP05, you have plenty of free memory to run even more powerful programs. The front panel can be protected to withstand adverse conditions (IP65).

Fitted with a backup battery, the panel can store all your backup data (Millenium 3 data, clock data, internal MTP05 data and alarm history) in the SRAM in the event of power failure.

About Crouzet

Crouzet, headquartered in France, has about 1,650 employees with a presence in more than 40 countries. Now known as a specialist brand, Crouzet is focused on added value and customization for integrators and equipment manufacturers. Crouzet provides products and solutions to the industrial, transportation, military and aerospace markets. www.crouzet.com

About Custom Sensors & Technologies

Headquartered in Moorpark, California, Custom Sensors & Technologies (CST) is made up of the leading brands of Crouzet, Kavlico and Crydom, as well as the former divisions of BEI Technologies, including Newall and Systron Donner. CST provides sensors, controls and actuation products to the industrial, transportation, military and aerospace markets. www.cstsensors.com

Email Newsletter icon, E-mail Newsletter icon, Email List icon, E-mail List icon

Signup for our industry newsletter.

Constant Contact SafeSubscribe