Corporate NewsTransportation NewsIndustrial NewsAerospace & Defense NewsNewsletters

For more information, please contact:

Gabriela Miranda

Crydom
T 619-210-1556
gabriela.miranda@crydom.com

Crydom Introduces Their New High Power PCB Mounted DC Output Solid State Relay (SSR)

August 26, 2009

High Power PCB Mounted DC Output Solid State Relay (SSR)

San Diego, CA – Crydom, a company of Custom Sensors & Technologies (CST) and a global expert in solid state relay Technology, introduces the CMX100D10, a high power PCB mounted DC output SSR. Crydom’s CMX Series of FET output printed circuit board mounted DC solid state relays previously rated to 6 amps at 100 VDC now includes a new model rated 10 amps at 100 VDC and 40°C ambient temperature. The CMX100D10 complements the CMX series that features models rated from 5 to 20 amps at 60 VC, 6 to 10 amps at 100 VDC, and 3 amps at 200 VDC.

All Crydom CMX series SSRs feature outputs with low on-state resistance FETs for efficient DC load control, 2500 VAC optical isolation, logic compatible DC control input and industry standard PCB mounting footprint in an epoxy package designed for full output rated operation at 40°C ambient temperature.

Crydom output SSRs are ideal for heating, lighting and motion control applications in industrial, medical, aerospace, rail, and automotive applications.

For more information on the new CMX100D10, contact the nearest Crydom Distributor, Representative or Local Crydom Sales Office, or visit Crydom website at www.crydom.com.

About Crydom

Crydom is an operation of Custom Sensors & Technologies (CST). Crydom is the global leader in solid state relay technology. Crydom manufactures and sells two of the most preferred brands of solid state relays around the world, Crydom and Crouzet. Thousands of catalog off-the-shelf items are available, as well as custom-designed solid state relays and related products. Crydom continues to satisfy the most demanding customers’ environmental and performance requirements creating product solutions to suit their specific application. www.crydom.com

About Custom Sensors & Technologies

Moorpark, CA – Custom Sensors & Technologies (CST) is a global business unit of Schneider Electric and is comprised of industry-leading brands including Crouzet, Kavlico, Crydom, and former divisions of BEI Technologies – Newall and Systron Donner. CST provides sensors, controls, and actuation products for the Transportation, Industrial and Aerospace & Defense markets. www.cstsensors.com

Email Newsletter icon, E-mail Newsletter icon, Email List icon, E-mail List icon

Signup for our industry newsletter.

Constant Contact SafeSubscribe