Corporate NewsTransportation NewsIndustrial NewsAerospace & Defense NewsNewsletters

For more information, please contact:

Gabriela Miranda

Crydom
T 619-210-1556
gabriela.miranda@crydom.com

Crydom Introduces 3 New DIN Rail Mounted High Power DC Output Solid State Relays

The new CKM Series expands Crydom’s broad line of DIN rail mounted SSRs with the addition of three new 22.5 mm wide models
rated for 10, 20 or 30 amps at 60 VDC for heating, lighting and motion
control applications

August 31, 2009

3 New DIN Rail Mounted High Power DC Output SSRs

San Diego, CA – Crydom, a company of Custom Sensors & Technologies (CST), and global expert in solid state relay technology, introduces the CKM series of FET output DIN rail mounted DC Power SSRs that are rated up to 30 amps/60 VDC at 40°C ambient temperature.

Mounting on industry standard 35 mm DIN rail, the Crydom CKM series SSRs with integral heat sink offer 2500 VAC optical coupling and logic compatible current regulated 4 to 32 VDC inputs with LED status indicator in a 22.5 mm wide “ready to use” assembly. Utilizing low on-state resistance FETs, the CKM series provides efficient and reliable DC load control for a wide range of applications including heating, lighting and motion control.

For more information on the CKM series contact the nearest Crydom Distributor, Representative or Local Crydom Sales Office, or visit our website at www.crydom.com.

About Crydom

Crydom is an operation of Custom Sensors & Technologies (CST). Crydom is the global leader in solid state relay technology. Crydom manufactures and sells two of the most preferred brands of solid state relays around the world, Crydom and Crouzet. Thousands of catalog off-the-shelf items are available, as well as custom-designed solid state relays and related products. Crydom continues to satisfy the most demanding customers’ environmental and performance requirements creating product solutions to suit their specific application. www.crydom.com

About Custom Sensors & Technologies

Moorpark, CA – Custom Sensors & Technologies (CST) is a global business unit of Schneider Electric and is comprised of industry-leading brands including Crouzet, Kavlico, Crydom, and former divisions of BEI Technologies – Newall and Systron Donner. CST provides sensors, controls, and actuation products for the Transportation, Industrial and Aerospace & Defense markets. www.cstsensors.com

Email Newsletter icon, E-mail Newsletter icon, Email List icon, E-mail List icon

Signup for our industry newsletter.

Constant Contact SafeSubscribe