Corporate NewsTransportation NewsIndustrial NewsAerospace & Defense NewsNewsletters

For more information, please contact:

Lori Appel
Manager, Marketing Communications

Kavlico
T 805-552-3406
F 805-523-7125
lappel@kavlico.com

Kavlico Introduces a Low Range Dual Channel High Pressure Sensor for Aircraft Hydraulic & Fuel Systems

September 3, 2009

Low Range Dual Channel High Pressure Sensor for Aircraft Hydraulic & Fuel Systems

MOORPARK, Calif. – Kavlico, a global business unit of Custom Sensors & Technologies (CST) has recently introduced a highly reliable dual channel pressure sensor that can measure pressures up to 4,000 PSIA or 275 Bar. The lightweight (6.5 oz. max.) aluminum housing has been designed to minimize weight; while the small footprint reduces installation time as only one sensor is now required for two measurements. With only one dual channel sensor to install vs. two single channel sensors, cabling requirements and costs are reduced resulting in a cost-effective sensing solution.

Utilizing Kavlico’s media isolated, oil-filled, piezo-resistive (PRT) sensing technology, the senor is capable of operation in harsh, flight critical environments with a typical MTBF of 300,000 hours at nominal operating temperatures. Each of the channel pressures are independent of one another, allowing the channels to be calibrated with different pressure outputs for each based upon the application-specific requirement of the aircraft platform. Burst pressure is nearly 2X the URL, and the operating temperature is -67° to +257°F.

Operating on a supply voltage of 5 to 15 Vdc, the sensor provides a non-amplified 0-100 mV output at 10 Vdc excitation. Sensor accuracy is ±1% of full scale output (FSO) over an operating temperature range of 0 to 200°F.

Typical applications include landing gear and control surface hydraulic systems as well as oil and fuel systems for commercial, civil/regional, and military aircraft. Custom pressure ranges and an amplified output of 0.5 to 4.5 Vdc with a power supply of 7 to 16 Vdc are available options for high volume OEM’s.

About Kavlico

Kavlico is an operation of Custom Sensors & Technologies (CST). Kavlico is a leading manufacturer of pressure, position (LVDT & RVDT), force, level, tilt, media quality, and other specialty sensors, and transducers for the transportation, industrial and aerospace & defense markets. www.kavlico.com

About Custom Sensors & Technologies

Headquartered in Moorpark, CA, Custom Sensors & Technologies (CST) unit is comprised of the industry-leading brands of Crouzet, Kavlico, Crydom, as well as the former divisions of BEI Technologies, including Newall and Systron Donner. CST provides sensors, controls, and actuation products for the transportation, industrial and aerospace & defense markets. www.cstsensors.com

Email Newsletter icon, E-mail Newsletter icon, Email List icon, E-mail List icon

Signup for our industry newsletter.

Constant Contact SafeSubscribe