Corporate NewsTransportation NewsIndustrial NewsAerospace & Defense NewsNewsletters

For more information, please contact:

Danny Donaldson

Newall
T 614-771-0213
ddonaldson@newall.com

Newall Launches New Generation of DRO Linear Encoder

September 24, 2009

New Generation of DRO Linear Encoder

Columbus, Ohio – Newall, a business unit of Custom Sensors & Technologies, has recently launched the Spherosyn 2G, a second generation linear encoder designed for the conventional machine tool market. The Spherosyn 2G is quick & east to install, requires no maintenance, and comes with a five-year warranty on the encoder and a lifetime warranty on the scales.

Newall’s linear encoder and scales technology is unique and provides consistent accuracy even under the harshest working environments. The new Spherosyn 2G encoder has completely new electronics and offers a significantly reduced total cost of ownership compared to its predecessor. The new internals enable more accurate alignment, which makes installation easier and 30 – 50% quicker than traditional technologies such as glass and magnetic tape.

With all the electronics encased in a new tough metal reader head, the Spherosyn 2G encoder and stainless steel scales require no maintenance whatsoever. The bushing technology and no mechanical wear characteristics mean it is extremely durable and reliable, giving minimal machine downtime.

Unlike glass scales which require regular cleaning and are susceptible to scratches or breaks, Newall’s robust stainless steel scales do not suffer from contamination problems and therefore don’t have to been cleaned or replaced. This alone can save thousands of pounds a year in machine shop overheads.

About Newall

Newall Measurement Systems, Ltd. was founded in 1968 in Peterborough, United Kingdom. Since that time Newall has dedicated itself to providing the machine tool and other machinery and production industries with leading edge technologies that increase productivity and machine tool efficiency. Over the years, Newall has grown to be a well-respected leader in digital readout systems and linear encoder technology. Over 85% of Newall’s products are exported, with distribution and service outlets in over 63 countries. www.newall.com

About Custom Sensors & Technologies

Headquartered in Moorpark, CA, Custom Sensors & Technologies (CST) unit is comprised of the industry-leading brands of Crouzet, Kavlico, Crydom, as well as the former divisions of BEI Technologies, including Newall and Systron Donner. CST provides sensors, controls, and actuation products for the transportation, industrial and aerospace & defense markets. www.cstsensors.com

Email Newsletter icon, E-mail Newsletter icon, Email List icon, E-mail List icon

Signup for our industry newsletter.

Constant Contact SafeSubscribe