Corporate NewsTransportation NewsIndustrial NewsAerospace & Defense NewsNewsletters

For more information, please contact:

Michelle Todd

BEI Industrial Encorders
T 800-350-2727
michelle.todd@beisensors.com

BEI’s Programmable Encoder Offers Simplicity and Convenience

October 21, 2009

 Programmable Encoder Offers Simplicity and Convenience

GOLETA, Calif. – BEI Industrial Encoders introduces the Omnicoder®, an incremental encoder that allows users to easily program the resolution anywhere between 1 and 10,000 counts per turn. Packaged in BEI’s flagship Model H25® encoder, the Omnicoder allows for virtually unlimited resolution variations.

Users can produce a wide range of resolutions from one encoder and it can be reprogrammed as needed to change the resolution. The Omnicoder programs over its existing M18 connector. Using an M18-to-USB programming cable, simply plug the Omnicoder directly into any PC. The programming software automatically detects the Omnicoder, then you simply type in the desired resolution, click the “Program” button and you’re done. It’s that simple.

Equipment can often have many encoders with various resolutions providing feedback to the control system. Omnicoder units can be kept on the shelf and programmed as needed. Users simply program an Omnicoder for the appropriate resolution and equipment is up and running in no time. This not only reduces machine downtime, but saves on inventory costs as well.

For more information, visit www.beiied.com/omnicoder

About BEI Industrial Encoders

BEI Industrial Encoders (IED) is a company of Custom Sensors & Technologies (CST). IED manufactures optical encoders and associated electronics for the industrial market. IED is the market-leading brand of encoders in North America. http://www.beiied.com

About Custom Sensors & Technologies

Headquartered in Moorpark, CA – Custom Sensors & Technologies (CST) is comprised of industry-leading brands including Crouzet, Kavlico, Crydom, and former divisions of BEI Technologies – Newall and Systron Donner. CST provides sensors, controls, and actuation products for the Transportation, Industrial and Aerospace & Defense markets.http://www.cstsensors.com

Email Newsletter icon, E-mail Newsletter icon, Email List icon, E-mail List icon

Signup for our industry newsletter.

Constant Contact SafeSubscribe