For more information, please contact:
Lori Appel
Manager, Marketing Communications
Kavlico
T 805-552-3406
F 805-523-7125
lappel@kavlico.com
November 1, 2009

MOORPARK, Calif. – Kavlico, a global business unit of Custom Sensors & Technologies (CST), has designed a sensor to measure common-rail pressure in diesel engines. The advantages of monitoring common rail pressure are many; including increasing engine power & torque, improving fuel economy, reducing engine noise, and improving vehicle drive-ability while creating cleaner exhaust emissions. With today’s restrictive emissions standards, keeping exhaust particulate emissions within the mandated levels is a must… and Kavlico’s common-rail sensor is an essential element of the common-rail injection system.
Pressure is regulated and monitored by the Electronic Diesel Control Unit (EDCU) which receives an electronic input from the Kavlico pressure sensor. The sensor operates on 5 Vdc and provides a 0.5 to 4.5 Vdc linear amplified analog output proportional to pressure to the EDCU. The highly accurate and ruggedly designed sensor uses a thin film TiON sense element which provides highly reliable and repeatable measurements.
The cost-effective sensor is EMI/EMC protected, has low power consumption, and is capable of operation in high vibration environments. Fully temperature compensated across the entire measurement range, the sensor has an operational temperature of -40°C to 125°C.
Pressure ranges are available from 0 to 3,000 Bar or 40,000+ PSI. The sensor can be customized to accommodate a wide array of pressure ports and electrical connector options dependent upon each OEM application-specific requirement. Alternative pressure ranges and output formats are also available upon request.
Kavlico is an operation of Custom Sensors & Technologies (CST). Kavlico is a leading manufacturer of pressure, position (LVDT & RVDT), force, level, tilt, media quality, and other specialty sensors, and transducers for the transportation, industrial and aerospace & defense markets. www.kavlico.com
Headquartered in Moorpark, CA, Custom Sensors & Technologies (CST) unit is comprised of the industry-leading brands of Crouzet, Kavlico, Crydom, as well as the former divisions of BEI Technologies, including Newall and Systron Donner. CST provides sensors, controls, and actuation products for the transportation, industrial and aerospace & defense markets. www.cstsensors.com