For more information, please contact:
Lori Appel
Kavlico
T 805-552-3406
F 805-523-7125
lappel@kavlico.com
June 5, 2007
MOORPARK, Calif. – Kavlico, an operation of Schneider Electric and a global business unit of Custom Sensors & Technologies (CST) is pleased to announce the release of their P4100 Board Mount Pressure Sensor with Quick-Hose Disconnect.
The small, yet robust sensor can be specified in pressure ranges of 0-15 to 0-300 PSI gage or absolute, operates on a 5 Vdc power supply and provides a linear amplified voltage output proportional to pressure of 0.5 to 4.5 Vdc.
Designed to measure dry air or inert gases, this compact and durable sensor is ideal for braking, active suspension, and other vehicle air pressure applications.
The quick-disconnect is an economical and handy feature that helps eliminate the cost of redundant air hose adapters, fittings, and reducers. A variety of quick-disconnect port sizes can be specified including 5/32”, 3/16” and ¼” among others.
The compact, lightweight and highly reliable design utilizes Kavlico’s field-proven piezoresistive sensing technology, which provides excellent EMI performance.
Kavlico is an operation of Custom Sensors & Technologies (CST). Kavlico manufactures high volume, application specific pressure, position, force, and specialty sensors for the transportation, industrial, and aerospace market sectors. www.kavlico.com
Custom Sensors & Technologies (CST) is a division of Schneider Electric and was formed from the combination of BEI Technologies, Kavlico, and Crouzet. CST provides sensors, controls, and actuation products to the industrial, transportation, and aerospace & government/military markets. www.cstsensors.com