Corporate NewsTransportation NewsIndustrial NewsAerospace & Defense NewsNewsletters

For more information, please contact:

Lori Appel

Kavlico
T (805) 523-2000 ext. 2206
F 805-523-7125
lappel@kavlico.com

Differential Pressure Sensors are Ideal for Diesel Particulate Filter Monitoring

November 21, 2007

Differential Pressure SensorsMOORPARK, Calif. – Kavlico, an operation of Schneider Electric and a global business unit of Custom Sensors & Technologies (CST) has designed a differential sensor for use with after-treatment systems to monitor particulate mater (PM) in diesel engine exhaust. Mandated by EPA regulations, Kavlico provides multiple pressure sensor solutions for the emerging emissions monitoring market. These sensors communicate data to determine when the system should regenerate or burnout toxic exhaust particles from the DPF filter.

These robust Diesel Particulate Filter (DPF) sensors incorporate a highly reliable and field-proven, ceramic capacitive sensing element. They provide a linear amplified output signal of 0.5 to 4.5 Vdc, which is proportional to pressure. Other features include EMI/RFI, reverse polarity and short circuit protection.

These highly accurate devices are designed to measure 0 to 750 mbar and have a proof pressure of 2 bar. The sensors have an operating temperature range of -40° to +125°C and can withstand the high vibration environment often found in on & off-highway vehicle applications. The rugged composite housing is well suited to operate in exhaust media settings where corrosion durability is required due to high soot, gas and acid levels.

About Kavlico

Kavlico is an operation of Custom Sensors & Technologies (CST) and is a global business unit of Schneider Electric. Kavlico is a leading manufacturer of pressure, position (LVDT & RVDT), force, level, tilt, media quality, and other specialty sensors and transducers for the transportation, industrial, and aerospace & defense markets.
www.kavlico.com

About Custom Sensors & Technologies

Headquartered in Moorpark, CA, Custom Sensors & Technologies (CST) is a global business unit of Schneider Electric and is comprised of the industry-leading brands of Crouzet, Kavlico, Crydom, as well as the former divisions of BEI Technologies, including Newall and Systron Donner. CST provides sensors, controls, and actuation products for the transportation, industrial, and aerospace & defense markets.
www.cstsensors.com

Email Newsletter icon, E-mail Newsletter icon, Email List icon, E-mail List icon

Signup for our industry newsletter.

Constant Contact SafeSubscribe