For more information, please contact:
Phil Roessler
Kavlico
T (805) 523-2000 ext. 2425
F 805-523-7125
proessler@kavlico.com
June 6, 2007
MOORPARK, Calif. – Kavlico, an operation of Schneider Electric and a global business unit of Custom Sensors & Technologies (CST) is pleased to announce that they have been chosen to supply the ARJ21 Regional Jet with its Landing Gear Control Lever (LGCL).
This robust device features a solenoid-actuated latch that prevents inadvertent gear up movement. The solenoid inside the LGCL is controlled by signals from the steering control unit to ensure that the lever is held in the down position while the aircraft is on the ground.
Other LGCL features include:
Kavlico is an operation of Custom Sensors & Technologies (CST). Kavlico manufactures high volume, application specific pressure, position, force, and specialty sensors for the transportation, industrial, and aerospace market sectors. www.kavlico.com
Custom Sensors & Technologies (CST) is a division of Schneider Electric and was formed from the combination of BEI Technologies, Kavlico, and Crouzet. CST provides sensors, controls, and actuation products to the industrial, transportation, and aerospace & government/military markets. www.cstsensors.com