For more information, please contact:
Phil Roessler
Kavlico
T (805) 523-2000 ext. 2425
F 805-523-7125
proessler@kavlico.com
June 6, 2007
MOORPARK, Calif. –Kavlico, an operation of Schneider Electric and a global business unit of Custom Sensors & Technologies (CST) is pleased to announce that they have been chosen to supply the ARJ21 Regional Jet with its Steering Handwheel (SHW).
This robust device features a non-contacting RVDT (Rotary Variable Differential Transformer) for reliable and accurate feedback of the handle position as it is rotated. In addition, the SHW contains a micro-switch to enable the steering handle to become active as it is depressed.
The SHW is painted to match the cockpit interior, is a line replaceable unit (LRU), and has been engineered, designed, and manufactured to meet the life of the aircraft. The SHW connector configuration allows for quick and easy installation to the power and control signals.
Kavlico is an operation of Custom Sensors & Technologies (CST). Kavlico manufactures high volume, application specific pressure, position, force, and specialty sensors for the transportation, industrial, and aerospace market sectors. www.kavlico.com
Custom Sensors & Technologies (CST) is a division of Schneider Electric and was formed from the combination of BEI Technologies, Kavlico, and Crouzet. CST provides sensors, controls, and actuation products to the industrial, transportation, and aerospace & government/military markets. www.cstsensors.com